Product Changes
Notification of Change
Swagelok has earned a reputation for unmatched quality and consistency at the component level. We are committed to maintaining this reputation while continuing to grow and improve our product offering. At times, this requires changes to the form, fit or function of our core products.
This Notification of Change sets forth changes to one or more of the products you may have purchased from Swagelok or an authorized Swagelok sales and service center. Prior to release, each change listed was carefully evaluated in accordance with the Swagelok Quality System, to minimize impact to you, our end customer.
A Notification relates to an applicable* change impacting Form, Fit and/or Function ("FFF") or the cosmetic appearance of a standard product. "Standard product" is any product that does not include a customer specified product or process attribute and can be purchased by any customer. This includes off-catalog product that can be assembled through designators, assemble to order ("ATO"), make to order ("MTO"), product produced by other means.
Unless otherwise noted, all changes are rolling changes and will take some time to flow through our global inventory. If you have questions regarding the impact of this change on your applications, please contact your local authorized Swagelok sales and service center representative. They, along with regional technology centers, and trained field engineers, are available to assist you.
The Following Changes have been Implemented
Effective Date: February 27th, 2024
Pressure Relief Valve Wire Locking Option
The Swagelok® pressure relief valve (PRV) wire locking option has recently received a process improvement. This new process will produce a more compact, twisted wire as shown in the images below. This change will have no impact to performance. The new process has been implemented, so future orders will be produced with the twisted wire, effectively immediately.
Effective Date: February 14th, 2024
DF Valve Flow Increase
As part of our continued review of products, the DF series high-flow, springless diaphragm valves will undergo the following changes:
The current geometry, a flat surface in the wetted area of the valve, will be phased out by part number starting June 1, 2024. The new geometry will increase the valve’s flow coefficient (Cv)by a minimum of 10%. During the transition, DF series valves may contain both geometries until inventory has been depleted. A visual change will only be detectable on the internals of the body component. To help differentiate between styles, a visual indicator will be added to the part.
The High-Flow, Springless Diaphragm Valves, DF Series catalog (MS-02-24) is being updated within the month of February to reflect this change. All other ratings remain unchanged, and all part numbers remain unchanged.
Effective Date: January 2nd, 2024
FDA Compliance Removal from FKM TS Gaskets
Swagelok FKM TS gaskets will no longer be FDA compliant or carry USP approvals on any orders placed after January 2nd, 2024. This will not affect the EPDM or PTFE gasket compliance status. The catalog (MS-03-13, page 2) is in process of being updated to reflect the following change in specification:
Item | Material | Specification |
Ferrules | 316L Stainless Steel | ASME-BPE |
Gaskets | PTFE (White) |
FDA 21CFR Part 117.1550 USP <88> Biological Reactivity Class VI USP <87> Cytotoxicity <Grade 2> |
EPDM |
FDA 21CFR Part 177.2600 USP <88> Biological Reactivity Class VI USP <87> Cytotoxicity <Grade 2> |
|
Fluorocarbon FKM (Brown) |
None
|
Any orders placed prior to January 2nd will maintain the FDA compliance until our current inventory is depleted. At inventory depletion, a freeze on orders of that gasket(s) will be instated until January 2nd when new material will be available without the FDA compliance.
Effective Date: Immediately
Thermoplastic Hose Changes: Replacement 7N and 7R Hoses / Discontinued Hoses
Swagelok's supplier has discontinued its production of thermoplastic hose series 7N and 7R. As a result, the Hose Service Group (HSG) was required to find a new supply to maintain these products in our standard offering. Although new products were obtained and validated with our existing end connections, they do not meet pressure requirements when swaged. Therefore, all customer swaging for 7N and 7R will have to be discontinued once the current hose inventory is exhausted.
The new bulk hose will meet all existing performance parameters, such as burst, temperature rating, and bend radii, and have the same lay line marking. However, the hose does have a dull finish as compared to the existing glossy cover. Please note this supply change does not impact 8R, 7P, and NG thermoplastic hose series.
The supply of 3/4" and 1" thermoplastic hoses in the 8R and 7P series has been discontinued and there are no suitable replacements for these products with our end connections. Therefore, 7P12, 7P16, 8R12 and 8R16 hoses will be removed from the standard Swagelok product offering once inventory is depleted. Thermoplastic end connections in those sizes will also be discontinued as a result.
Effective Date: January 1st, 2024
Removal Generic Patented Related Markings
As part of Swagelok’s ongoing commitment to continuous improvement, we will begin to phase out generic patented and outdated patent pending related markings on all parts and products. Legal statements of Swagelok products being covered by patents will remain in product literature. A visual change may be noticeable on the products. This running change will begin in January 2024. During the transition, shipments may contain both versions until stock has been depleted.
Effective Date: January 1, 2024
Discontinuation of select Swagelok Process Interface and Process Monoflange Valve Products
In conjunction with agile supply chain management changes for Swagelok Process Interface and Process Monoflange Valve products, VB0451 and VB05 will be discontinued. Furthermore, the process interface valves, double block and bleed (DBB) valves catalog, MS-02-340, is being updated and will be completed in advance January 1, 2024. It will reflect a change to Swagelok order numbering for Swagelok Process Interface and Process Monoflange Valve Products (e.g., VB04 will change to VS04).
Effective Date: November 7, 2023
“B” Type VCO L-Ring Seals Being Discontinued
Description of Change: As part of our continued review of products that support Swagelok's strategic plans, the L-Ring seals for the “B” Type VCO (BVCO) fittings will be discontinued once current inventory is depleted. This notice is a follow up to the “B” Type VCO fittings obsolescence which was posted in 2021.
BVCO L-Ring seals will no longer be available for order November 7, 2023. All existing acknowledged BVCO L-ring orders will be fulfilled.
Effective Date: Immediately
Select Needle and Metering Valves Being Discontinued
In alignment with our commercial strategy to simplify existing products to drive availability, we will be obsoleting the product series below. These products have had limited sales and have existing alternatives with similar performance. Orders will be accepted with no restrictions until November 1, 2023. Orders will be accepted only for remaining inventory from November 1, 2023, until April 1, 2024. Valves being discontinued:
- All screwed-bonnet needle valves, JB series
- All screwed-bonnet needle valves, JN series
- Metering valves, L series only (no changes to the S, M, and 31 series)
Customers may consider alternative valve products including M, 31, or 1 Series valves
Effective Date: Various noted below
2D (Two-Dimensional) Barcodes Added to Additional High Purity Products
One of the ways Swagelok lives its core value of quality is to implement technologies that help enhance product quality. Establishing a unique identification number for each valve body and applying a 2D barcode to the product allows the product’s progress to be tracked through assembly operations. This unique ID also links the valve to a rigid verification process to ensure the valve’s assembly to factory specifications.
Starting in 2012, we began applying 2D barcodes to select high purity products.
HF Regulators: Effective September 1, 2023, 2D barcodes will be applied to HF series regulators.
DH Valves: In 2018, 2D bar codes were added to certain DH process sheet valves. Effective February 1, 2024, 2D barcodes will be applied to all DH series valves.
There are no other changes to the product marking. Product will transition over time so both marking styles may be seen in shipments until current inventory is depleted. We continue to investigate adding a 2D barcode to other products and expect to implement it on more products in the coming months.
Important: Although 2D barcodes are similar in appearance to QR (Quick Response) codes used in various media, the underlying code language is different. Specific equipment is needed to read the 2D barcode.
Effective Date: May 18th, 2023
Select Exotic Alloy B Series Valves Being Discontinued
Select exotic alloy B series bellows-sealed valves and kits will be discontinued once current inventory is depleted.
- 6B and 8B alloy 400 valves, fractional and metric.
- Select 4B alloy 400 valves - M-4BMG, M-4BMW, M-4BRG, M-4BRG-SC11, M-4BRG-V51, M-4BRW, M-4BRW-TW, M-4BRW-V51
- All B series valves with a stainless steel body and alloy 600 bellows, fractional and metric.
Refer to Bellows-Sealed Valves, B Series, MS-01-22, for additional information on B series valves.
As an alternative, Swagelok offers U series bellows-sealed valves with alloy 600 bellows. U series bellows-sealed valves ordered with an alloy 400 body are assembled as standard with alloy 600 wetted components. Refer to the U Series catalog, Bellows-sealed Valves, U Series (MS-01-38), for additional material of construction information.
Effective Date: February 2023
HB Series Bellows Replacement Kit Instruction Card Updated
We have updated the HB series instruction card, HB Series Pneumatically Actuated Valve Bellows Subassembly and Gasket Replacement Instructions (MS-CRD-0023), to include the use of either a 5/16 in. or an 8 mm hex nut driver to service the bellows subassembly.
Effective Date: Effective Immediately
DRP Series Diaphragm Valve Injection Molded Components
In the spirit of continuous improvement and quality, we are updating the DRP series injection molded components to improve the injection molding process. The mold updates may result in visual changes for all DRP size offerings (DRP4, DRP8, and DRP16) but do not affect the valve function.
Examples of these changes include changes to molding gates, coring, ribbing, drafts, and radii as well as the one-quarter inch, 3-way pneumatically actuated hole plugs being reduced to match the 2-way hole plugs. These non-wetted polypropylene components are listed in the Materials of Construction table of the DRP series catalog, MS-02-171.
Effective Date: Effective Immediately
PTX Digital Pressure and Temperature Transducers / VCM Digital Valve Control Module
Due to critical component unavailability, the PTX series transducer will be discontinued effective immediately. Swagelok will also be discontinuing the VCM series. We will continue to accept limited orders for VCM and final purchases until the existing inventory has been depleted, or through the end of 2022, whichever occurs first.
Effective Date: Effective Immediately
Swagelok’s Ratchet Wrenches to be Discontinued
Due to discontinuance by the supplier and the absence of alternative suppliers, RW series ratchet wrenches and holding pouch will no longer be sold after remaining inventory has been depleted.
The product catalog, Gaugeable Tube Fittings and Adapter Fittings, MS-01-140, will be updated to remove this product offering.
Effective Date: December 2, 2022
DR Series Diaphragm Valves Being Discontinued
The DR series radial diaphragm valves will be discontinued. While no direct replacement exists, Swagelok will continue to offer DR diaphragm replacement kits (ordering numbers listed below) for a minimum of 2 years. DR diaphragm valves will no longer be available for order as of December 2, 2022. Reference Radial Diaphragm Valve, DR Series, MS-02-186, for additional information on DR series valves.
DR Diaphragm Replacement Kits: NXT-3DK-DR8, NXT-3DK-DR12, NXT-3DK-DR16, NXT-3DK-DR24, NXT-3DK-DR32
Effective Date: Effective Immediately
Carbon Steel GU Series Needle Valves and SBV Subsea Service Ball Valves
Swagelok will no longer offer carbon steel as a material option for the GU Series Needle Valve. An example part number for this material option would be as follows: S-4GUF8.
We will continue to offer GU Series Needle Valves in 316 Stainless Steel material. Please reference General Utility Service Needle Valves, MS-02-312, for additional information on the stainless steel option for the GU Series Needle Valve.
In addition, Swagelok will also discontinue sales of the SBV Subsea Service Ball Valve. Please reference Medium- and High-Pressure Fittings, Tubing, Valves, and Accessories, MS-02-472, for additional information on the SBV Subsea Service Ball Valve.
Effective Date: Effective Immediately
NACE MR0175/ISO 15156 Update for 316/316L, 6MO Pipe and 316/316L FK Fittings
Updates have been made to the NACE MR0175/ISO 15156 International Standard: tables A.4 and A.11 for 316/316L Stainless Steel and 6-Moly fitting materials, enabling increased product availability. Effective immediately, Swagelok stainless steel and 6-moly pipe and medium-pressure FK fittings produced using material in the cold-drawn condition will be NACE MR0175/ISO 15156 compliant.
The above changes were driven by Technical Circular ISO 15156-3:2020/Cir.1:2021(E), Petroleum and natural gas industries — Materials for use in H2S-containing environments in oil and gas production — Part 3: Cracking-resistant CRAs (corrosion-resistant alloys) and other alloys.
Technical Bulletin MS-06-124, NACE® MR0175/MR0103 and ISO 15156/ISO 17945 Compliant Swagelok® Fittings should be referenced for additional information relative to this change.
Effective Date: Effective Immediately
Discontinuation of Lanyard Tag with CRN Option for Hose (-CRN)
Swagelok will no longer be offering the -CRN suffix option on assembled hoses effective immediately. This change will NOT impact the CRN certification status of any hoses. Customers who wish to continue with receiving tags that have CRN information should consider the -T suffix option with the CRN data as the specified text on the tag.
Effective Date: August 2nd, 2022
DA Series Diaphragm Valves Being Discontinued 
The Swagelok DA series valve is now being formally discontinued and replaced with Swagelok’s DP Diaphragm Valve product line. Reference Springless Diaphragm Valves for High Performance, DP Series, MS-01-165, for additional information on the DP series valves.
DA diaphragm valves will no longer be available for order as of August 2, 2022. The DA diaphragm replacement kit (E-3DK-DA) will continue to be available until August 2, 2024.
Effective Date: Effective Immediately
Change to 8GB Series Locking Bracket Design – Notification of Change
A design change to the 8GB series locking bracket (“JL” option) was recently implemented to improve the handle clearance. This change has no impact on the functionality of the product or the installation instructions. The new screws use the same installation tools and procedure as the original design. Ordering numbers for the valve option (JL designator) and kit (SS-5DK-8GB-JL) will not change.
Effective Date: Effective Immediately
Change to QTM Series Quick-Connects Pressure and Temperature Rating – Notification of Change
We are pleased to inform you that the temperature rating of the PTFE sealed QTM series quick connect will increase from a maximum of 120°F (48°C) to a maximum of 350°F (176°C) at a pressure rating of 800 psig (55.1 bar). All other ratings will remain the same.
This change is a result of expanded validation testing of the current design. No design changes were made to the product in order to achieve this extended temperature rating.
The product literature, Quick-Connects, MS-01-138, has been updated. There are no changes to placing an order for these items.
Effective Date: January 1st, 2023
Changes to CE marked products entering the United Kingdom – Notification of Change
Certain products used in the United Kingdom (UK) and manufactured on or after this date will require a UK-CA marking in place of the current CE marking. Most of the products currently offered with CE marking as standard will be transitioning to have the CE and UK-CA marking as standard.
The following products currently marked with CE will be provided with dual CE/UK-CA marking as standard. No special designator will be required for these products.
- 67/68 series manual ball valves, RHPS series regulators, double block and bleed valves (VB) and monoflanges (MN)
- ISO 5211 compliant pneumatic actuators
- KEV Series Vaporizing Regulators
- Welding system (M200), MHSU, tube facing tool, and manual tube bender
The following products may need a special designator to be provided with the UK-CA mark instead of the CE-mark as of January 1, 2023:
- Rupture disks
- Gauges and transducers
We do not plan on pursuing UK-CA marking at this time for the following products. They will only be offered with CE-marking, which will be allowed for use in the UK until January 1, 2023.
- PRV relief valve
- Air actuated assemblies and 3rd party limit switches, solenoids, etc. (affects UK-CA and UKEx assemblies for explosive atmospheres)
- AHSU, cone/thread tool, electric tube bender, HVSU
- PTX, VAF, VCM smart products
Effective Date: November 1st, 2021
Product Marking Change for EC-79 Fittings – Notification of Change
Fittings certified to EC-79 will have a change in product marking, effective November 1, 2021. This change is the result of updated EC-79 certificate requirements. This change only affects fittings that contain the HV35 or HV70 designators in the ordering number. Markings will now be found only on the body of the fitting, opposed to both the body and the nut.
Effective Date: Effective Immediately
RC Marked Cylinders Being Discontinued – Notification of Change
We have offered “RC” marked cylinders for applications that require pressurized samples for transportation in other countries. Due to a new requirement for these applications that these cylinders must meet a specific requirement, this product is effectively no longer available. All other cylinders will continue to be offered as normal.
Effective Date: August 11th, 2021
Visual Change to Select Assembly-by-Torque (AbT) Fittings – Notification of Change
In the spirit of continuous improvement, customers may observe a change in product marking location on SS-4ABT1-1-0400 / SS-4ABT1-1-0400XR / SS-4ABT1-1-0401 / SS-4ABT1-1-0401XR / SS-4ABT1-1-4 AbT fittings.
These changes do not affect form, fit, or function of the product. No other AbT fittings are affected.
Effective Date: February, 2022
General Industrial Valve Component Material
Tetralon, a red-colored glass-filled PTFE material, is being discontinued by the current supplier and will be replaced by another glass-filled PTFE material. The new material will not contain the addition of an iron oxide pigment that gave Tetralon components a red color, resulting in a color change for the components listed below from red to white.
This change has no impact to product fit or function.
Valve Series/Components Impacted:
- N Series Severe-Service Union-Bonnet Needle Valves – stem packing supports
- V Series Instrument Manifolds – optional reinforced PTFE flange seal
- VE Series Instrument Manifold – optional glass filled PTFE bonnet seal packing
- 83 Series Trunnion Ball Valve – trunnion back-up ring and stem bearing (2 ways)
- H83 Series Trunnion Ball Valve – seat carrier back-up rings
- 131, 133 Series Pneumatic Actuators – thrust washers
Effective Date: Effective Immediately
Raw Material Source Change and Pressure Rating Update for J6 Manifolds
To improve delivery of J6 manifolds, Swagelok has changed raw material sources. Effective immediately, the manifold body for all J6 manifold assemblies will change from an extrusion to bar stock. Material composition is the same, and there is no impact to product performance. As a result of the change, the width of the manifold will increase from 2.36 in. (60mm) to 2.44 in. (62 mm).
An additional update has been made to the pressure rating for the 1 in. size end connection listed in catalog MS-02-214. The catalog previously stated a maximum working pressure of 2000 PSIG (137 BAR) at 200 °F (93 °C) for 1 in. size end connections. The catalog has been updated to reflect the actual rating of 3000 PSIG (206 BAR) at 200 °F (93 °C). All other pressure and temperature ratings remain the same.
Effective Date: June 14, 2021
"B" Type VCO L-Ring Face Seal Fittings Being Discontinued
“B” Type VCO fittings as well as valves with “B” Type VCO end connections will be discontinued and no longer be available for order as of June 14, 2021. “B” Type VCO L-ring seals will continue to be available until May 14, 2023. A follow-up notice will be issued in advance of the L-ring seal obsolescence. The standard VCO O-ring face seal fitting continues to be available.
Effective Date: Effective Immediately
Fluid Distribution Headers End Cap
To increase our ability to provide solutions meeting our customers’ needs in a timely fashion, Swagelok is modifying the FDH end cap configuration affecting many, but not all, of the FDH product assemblies.
Effective immediately we are implementing a change to FDH end caps that will maintain product flexibility while improving availability. For FDH1 manifolds, end caps and O-rings are no longer available. Instead, the ends of the manifold bodies will be threaded with ¾ in. female NPT. Alternative end connections are available by using adapter fittings.
For FDH2 manifolds, the number of end cap configurations has been reduced to better facilitate stocking. Like the FHD1, alternative end connections can be provided using adapter fittings. These changes does not affect FDH outlet connections.
FDH assembly ordering information is not affected. Customers should continue to select the desired FDH inlet and drain end cap connections using the existing ordering number designators.
Please be aware that the affected FDHs will be slightly longer due to the added adapter fittings. The Fluid Distribution Header Application Guide, MS-02-358, has been updated to reflect these changes.
Effective Date: May 28th, 2021
Gaugeable Preswage Tool to Replace Non-Gaugeable Version in Select Sizes
The following non-gaugeable preswage tool sizes will be discontinued: 1/4 in., 3/8 in., 1/2 in., 5/8 in., 6 mm, 8 mm, 10 mm, 12 mm, and 16 mm. The gaugeable version, which enables customers to quickly measure the gap between the nut and fitting body with a standard Swagelok gap inspection gauge during Swagelok tube fitting installation, will replace the discontinued non-gaugeable sizes. All other non-gaugeable preswage tool sizes are not impacted by this change and will continue to be available.
Please note: The instructions for the gaugeable pre-swage tool differ from those for the non-gaugeable tool. Reference catalog MS-01-140, Gaugeable Tube Fittings and Adapter Fittings, for non-gaugeable preswage instructions and instruction card MS-CRD-0110 for gaugeable preswage instructions.
Effective Date: April 16, 2021
ISO 5211-Compliant Pneumatic Actuator Instructions Move to QR Code – Notification of Change
Effective April 16, 2021, the maintenance and operating instruction manual for Swagelok-branded ISO 5211-compliant pneumatic actuators will be available via a Quick Response (QR) code only. To reduce environmental impact, a small printout of the QR code will replace the leaflet included with the actuator/valve packaging.
The following pneumatic actuator models are subject to this change:
- A10, A15, A30, A60, A100, A150, A220
- A15XD, A30XD, A60XD, A100XD
This change impacts the following ball valve product series with ISO 5211-compliant actuators:
- One-Piece Instrumentation Ball Valves—40G Series and 40 Series
- Ball Valves, General Purpose and Special Application—60 Series
- Trunnion Ball Valves—83 and H83 Series
- Swagelok Alternative Fuel Service (AFS) Ball Valves for High-Pressure, High-Flow Applications
- Multipurpose Ball Valves—SK Series
- Medium-Pressure Ball Valves—CTB/FKB Series
- General Service Ball Valves, GB Series
Effective Date: Immediately
Changes to Inductive Sensor Cable Overmold
The cable overmold on the inductive sensor used in select ALD and DP series valves will have a different cosmetic appearance. Recently, global cable availability has been limited, and to meet the current demand of this sensor, our supplier is using their approved secondary source of pre-molded cables. This cosmetic change does not impact the function of the product.
Effective Date: March 1st, 2021
Product Name: BY, CH, CW, R4, and RL3 Series Valves
Description and Reason for Change: To comply with updated environmental requirements, the bonding agent used on the bonded poppets and seats in select BY, CH, CW, R4, and RL3 series valves will change from Chemlok® 250X to Chemlok 6150. This will align Swagelok with international health and safety standards.
Note: This change does not impact product ratings.
BY Series | CH Series | CW Series | R4 Series; | RL3 Series | |
Elastomer Material | EPDM | Buna N Buna C EPDM Neoprene |
Buna N EPDM Neoprene |
Buna N Buna C EPDM Neoprene |
Buna N EPDM Neoprene |
Poppet Material | 316 SS | 316 SS Alloy 400 Alloy C276 |
316 SS | 316 SS | 316 SS |
Effective Date: January 5, 2021
Product Name: AFS and 40 Series Valves
Description and Reason for Change: In the spirit of continuous improvement, we are changing the nylon handles used on our standard AFS and 45 series ball valves by replacing the current brass handle insert with a more robust, stainless steel handle insert. The new handle will be easier to actuate and will incorporate the handle stop into the handle, removing the need for an additional handle stop insert.
This change will not affect the handle function or any valve ordering numbers. However, it will result in a change to the size of the handle used for 45 series valves and in handle kit ordering numbers. The new handle will carry the same dimensions as the current AFS series handle.
Made-to-stock valve orders may see the old handles until stock is depleted. If you require a 45 series valve with the old handle using the brass insert, we will continue to offer kits with the old handle (ordering number BZ-5K-45-BK) for up to two years. If a customer requires a valve assembled with the original 45 series handle, the local sales and service center must contact Swagelok Technical Service.
We are implementing the same change to existing 42, 43, and 44 series handles in Q2 2021, updating the handle insert from brass to stainless steel. This will make the handle consistent with the 40G handle design, which already includes the stainless steel insert. This will not change the fit or function of these valves, and there will not be any changes to end item or handle kit ordering numbers. The transition will be implemented as inventory is depleted and you may see shipments containing both handle types during this time.
Effective Date: November 17, 2020
Product Name: 43T Series Valve Packing Material
Description and Reason for Change: As part of Swagelok's ongoing commitment to implement continuous quality improvements to meet the performance needs of demanding applications, the upper and lower packing of the 43T series ball valve is changing from PFA to Modified PTFE/D1710 type 1, Grade 1, Class B material (TFM). The TFM material is the same material currently used in the 43G valve.
This change impacts the 2-way, 3-way, angle pattern, 4-way, and 5-way configurations of the 43T series ball valve only. The 43T series 6-way and 7-way configurations as well as 41, 42, 44, and 45 series valves are not impacted by this change at this time but may be evaluated for this change in the future. There will be no impact to valve fit/function, pressure/temperature ratings, or certifications. Valve ordering numbers will remain the same.
The implementation for this new packing will be a running change. As inventory of the PFA material is depleted, valve assemblies will transition to the new TFM material. Based on current inventory, the change in material will occur within approximately 6 months.
Until this transition is complete, it is possible that customers could receive valve orders assembled with either the PFA or the TFM material. Controls will be put into place to ensure there is no mixing of packing material within the same valve.
Effective Date: November 4, 2020
Product Name: BN Series Pneumatically Actuated Bellows Valve Stem
Description and Reason for Change: In the spirit of continuous improvement, we are implementing a change to all pneumatically actuated BN series valve stems. The upper part of the stem shank will now be thicker, improving our customers' ability to consistently install the retaining ring into the proper groove on the stem.
BN Valve
This change does not impact the function of the valve and will only be visually detectable during maintenance of the valve. This will begin in the next 30 days. During the transition, you may see shipments of assembled valves and maintenance kits containing both versions of the stem until the existing stock is depleted.
Description and Reason for Change: Small visual and chemical changes will be made to the Aflas® bonded poppet for the CW series check valve. These changes will enable Swagelok to secure long-term availability of the Aflas bonded poppet component. The visual changes are as follows and will be visible when looking though the inlet port:
- Aflas color will change from dark brown to black (ASTM D2000 material remains the same)
- A molding cavity number will be added under the “AF” material designator
Additionally, the adhesive of the bonded poppet will change from Chemlok® 8116 to Chemlok 5150 to meet updated environmental standards. The other CW series poppet materials will also change to this adhesive in the coming months. A notice will be released as that transition is completed.
None of these changes will impact the function of the product.
Product Name: 5 and 6 Series Actuators
Description and Reason for Change: In the spirit of continuous improvement and quality, we are implementing a change to all 5 and 6 series actuators by adding a bellows valve option, improving the thread engagement on the panel mount nut.
Currently, there is no counter-bore on the actuator base plate. Moving forward, all 5 and 6 series actuators will include a small counter-bore which will provide more space for the panel nut threads to engage. Please note this does not impact the function of the product.
During the transition over the next 30 days, both versions of the actuator will be shipped until the existing stock is depleted. Please note that all existing product without the counter-bore still meets Swagelok quality standards.
Product Name: Gaugeable Preswage Tool
Description and Reason for Change: The gaugeable preswage tool is moving from a one-piece body design to a two-piece design except for the 5/8 inch size, similar to the standard Swagelok preswage tool design. The new design uses a machined insert that is pressed into a cast body. This will result in an improvement in manufacturing output.
All functional dimensions are remaining the same. However, there will be a visual and physical difference for the tool (greater overall length and body diameter). There is no impact to product function. Ordering numbers will remain the same. Implementation for the change has begun and shipments of the new design will take place throughout October; we will be fully transitioned for the impacted sizes by the end of October.
Effective Date: August 14, 2020
Product Name: HK Series Bellows Valve Discontinuance
Description and Reason for Change: HK series brass and alloy 400 bellows valves will no longer be available after remaining inventory has been depleted. The raw material used in the production of the bellows has been discontinued and a new, robust supply chain is unavailable. The decision has been made to discontinue the product line as viable alternative products are available as listed below.
New requests will be fulfilled on a first-come, first-served basis until inventory is depleted. For applications requiring compact brass bellows valves, the brass BK series continues to be available. The H series stainless steel bellows valve will also remain available.
Please reference Bellows-Sealed Valves, H and HK Series, MS-01-36 for additional information on the H and HK series valves.
Effective Date: Q3, 2020
Product Name: T Series PTFE Hose
Description and Reason for Change: Swagelok's Hose Service Group is pleased to announce that the T Series BHT and MBHT hose will be transitioning from a swaged end connection to a crimped design starting Q3, 2020. As we make this transition, the configurable TH series hose will continue to have a swaged end connection until approximately Q1, 2021.
While this change will allow us to increase manufacturing efficiency, we also anticipate these advantages (see Hose and Flexible Tubing catalog - MS-01-180, for updated technical data):
- Improved product performance allowing for increased pressure ratings at elevated temperatures that will be updated, along with the product dimensions, in the Hose and Flexible Tubing catalog.
- Revised product dimensions
- Inclusion into local distributor crimp cell capabilities for local assembly.
- The transition to crimped components allow us to improve our traceability.
Crimped ends will be supplied as end connection inventory for swaged assemblies are depleted. You may see both designs in orders containing multiple end connection types until the transition is complete. TH series hose will continue to have a swaged end connection until approximately the beginning of 2021. More information regarding other versions will be released in a timely manner.
Effective Date: December 1, 2019
Product Name: T Series PTFE Hose
Description and Reason for Change: Swagelok's Hose Service Group is pleased to announce that the T Series PTFE hose will be transitioning from a swaged to a crimped design for assembly of end connections starting December 1, 2019.
While this change will allow us to increase manufacturing efficiency, we also anticipate these advantages:
- Improved product performance allowing for increased pressure ratings at elevated temperatures that will be updated, along with the product dimensions, in the Hose and Flexible Tubing catalog.
- Inclusion into local distributor crimp cell capabilities for local assembly.
The current swaged design will continue to be the only version supplied until December 1, 2019. Following that date, crimped ends will be supplied as end connection inventory of swaged assemblies are depleted. You may see both designs in orders containing multiple end connection types until the transition is complete.
Effective Date: August 30, 2019
Product Name: PB Series Rubber Hose
Description and Reason for Change: As a part of our effort to provide exceptional service to our customers and to facilitate ideal packaging of PB series hose and end connections, there is a change to the product line. Swagelok is making a design improvement on the end connections that will eliminate the finishing cap. This change will allow for bulk packaging, eliminating the need to cut open individual bags, and provide a cleaner visual appearance.
The removal of the finishing cap may require minor changes to the length and/or outside dimension of the end connection. An updated Hose and Flexible Tubing catalog is available and reflects the dimensional changes associated with the new end connection, as well as the visual changes due to the removal of the finishing cap.
The new supply of bulk hose may have minor visual differences specific to the color and surface finish. The same color options will be provided, however, there may be slight differences in the shade of the colors. The gray color hose will contain black text in place of white text. The black color bulk hose will be constructed with a Neoprene cover for added UV and ozone resistance. The hose reel size and/or material may also change.
These changes will go into effect no earlier than August 30, 2019. After this date, there will be a transition period where both end connection designs and bulk hose supplies could be used in orders as existing inventory is depleted.
Effective Date: September 30, 2019
Product Name: Swagelok Facing Tool Service Update for SWS-232EP Model
Description and Reason for Change:
Swagelok will no longer service the SWS-232EP model facing tool as of September 30, 2019, or until spare parts can no longer be supplied, whichever comes first. Sales of the SWS-232EP were discontinued in 2011 in conjunction with the release of the MS-TF series facing tools.
Swagelok continues to offer the MS-TF series facing tools. Refer to Tube Facing Tools, TF16, TF24, TF40, and TF72 Series, MS-02-426, for additional information on those models. We have continued service and support of the SWS-232EP facing tool since 2011. However, our suppliers are no longer able to supply components to meet our servicing commitments for the SWS-232EP.
Effective Date: July 1, 2019
Product Name: PB Series Rubber Hose End Connections
Description and Reason for Change:
As a part of our effort to provide exceptional service to our customers and to facilitate the packaging of PB series hose and end connections, two changes are being made to the product line. First, Swagelok is making a design improvement on the end connections that will eliminate the finishing cap. This change will allow for bulk packaging, eliminating the need to cut open individual bags by you or your customer, and provide a cleaner visual appearance. Second, we are moving the bulk hose product to a new supplier. The new supplier is already used for other Swagelok products.
Product ratings will be unchanged as the new supplier will meet the same performance requirements. Swagelok has validated both bulk hose suppliers for both end connection designs to ensure there is no concern for intermix between designs or suppliers. These changes will go into effect no earlier than July 1st, 2019. Following that date, there will be a transition period where both end connection designs may be received in orders as existing inventory is depleted.
Effective Date: January 9, 2019
Product Name: FKB Series Medium-Pressure Ball Valve Standard Handle
Description and Reason for Change:
Swagelok is continuously looking for ways to improve our products. The standard handle for the FKB series ball valve has been changed to incorporate a blue vinyl sleeve for increased gripping power, replacing the blue powder coating. These changes will improve functionality and simplify the standard product offering. The new handle is non-positionable. The positionable handle is available as an option.